changes – The Corporate Blog

Energy from the wind tree

From a distance it looks like a tree, but on closer inspection it turns out to be an innovative small-scale power plant: a wind tree that delivers sustainable electricity at Endress+Hauser in Gerlingen, Germany.

Eco power plant for the city: The wind tree supplies the e-vehicle charging station with electricity.
Eco power plant for the city: The wind tree supplies the e-vehicle charging station with electricity.

The wind tree is nothing more than a small wind power station, 9.9 meters high with a metal trunk and branches, adorned with vertical, green-colored plastic turbines that resemble large leaves from afar. Driven only by wind, the 54 approximately 85-centimeterhigh mini turbines rotate to generate electricity. With an electrical power of 4,000 watts, the turbines produce around 3,200 kilowatt hours of electricity per year, enough to supply a one-person household.

Compared to a large wind turbine, that doesn’t seem like much. But this small power plant offers key advantages. The small dimensions make it suitable for installation in urban environments, for example. The leaf-shaped turbines can also utilize any form of wind, even turbulent air flows that often occur in built-up areas. And they are nearly silent. Jérôme Michaud-Larivière, the inventor, estimates that his micro power station can operate 320 days a year in normal wind conditions, with a life cycle of 25 years. 

“The wind tree is a visible sign of our commitment to handle our environment and natural resources in a responsible manner,” says Manfred Jagiella, Managing Director at Endress+ Hauser Liquid Analysis. The company has implemented a sustainable energy concept for years. As part of the expansion and modification of the facility in Gerlingen, the building systems were designed for energy efficiency from the ground up, and are optimized on a continual basis.

Electric driving is now a beneficiary of the wind power station as the electricity flows directly into an innovative redox flow battery, which in turn supplies power to a charging station located in front of the building. “That means our own vehicles, as well as our visitors’ vehicles, can now operate with climate-friendly, autonomously generated energy,” says Manfred Jagiella.

1 Comment

  1. Scott Sutherland

    I would like to see one of these at the new Endress+Hauser campus in Houston. I have a Prius Prime ready for the first test!

    Reply

Leave a Reply to Scott Sutherland Cancel reply

Your email address will not be published. Required fields are marked *